Skip to main content

Arduino Library Setup

This section assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino IDE, library, or board add-ons, we recommend reading through the following tutorials.

SparkFun ADE7953 Arduino Library Installation

This library is built using the SparkFun Toolkit so you'll need to make sure that is installed before using this library. Install the SparkFun Toolkit with the Arduino Library manager by searching "SparkFun Toolkit" and installing the latest version. Users who prefer manually installing Arduino Libraries can download it from the GitHub Repository.

The SparkFun ADE7953 Arduino Library lets you quickly set up, configure and receive data from the ADE7953 and includes eight examples. Install the library using the Arduino Library Manager tool by searching for "SparkFun ADE7953" and install the latest version. If you'd prefer to manually install the library, you can download it from the GitHub Repository or you can download a ZIP of the repository here.